Press Releases
RS Components augments portfolio of electrical measurement equipment with five new ranges of intuitive testers from Testo
Electrical measurement devices provide affordable test capabilities for engineers working in HVAC design and maintenance
Singapore, 2 August 2016:
RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, is extending its portfolio of high-quality electrical test and measurement devices with five innovative product ranges from Testo. The devices offer measurement capabilities for a diverse variety of electrical systems and appliances, including for use by electrical installation contractors and engineers working in HVAC design and maintenance.
The Testo 760 is the industry’s first automatic digital multimeter range and provides functionality for all electrical measuring tasks, including function keys that replace the traditional dial for easier operation and greater reliability. Measurement parameters are detected automatically via the assignment of measuring sockets, therefore it is impossible to make incorrect settings. Three models are available: the standard Testo 760-1, which covers most daily measuring tasks; the Testo 760-2 offering TRMS measurement, an extended current range from µA up to 10A, and a low-pass filter, which allows technicians to take accurate voltage readings at variable frequency drives; and the high-specification 760-3, which has additional features including voltage up to 1000V and higher ranges for frequency and capacitance.
The Testo 770 clamp meter range is ideally suited to current measurement in switching cabinets, as the device’s unique grab mechanism allows one of the pincer arms to be fully retracted to capture cables in tight spaces. Automatic measurement parameter detection ensures reliable work enabling automation detection of DC and AC and the selection of other parameters such as resistance, continuity, diode and capacitance. It is available in three models: the standard 770-1; the 770-2, which includes a µA range and an integrated temperature adapter for all type K thermocouples; and the 770-3, which offers additional functions such as performance measurement and integrated Bluetooth, allowing the instrument to be connected to the Testo Smart Probes App. Use of the 770-3 and the Smart Probes App makes the daily work of a technician significantly easier and more efficient by providing several important measurement parameters via wireless communication in a single app. Within this app, measurement progression can be shown as a graph or a table and the results can also be directly communicated via email.
The Testo 755 current-voltage tester family is ideal for most daily electrical measuring tasks. Automatically selecting the right settings, the devices have all the important functions for determining voltage/de-energisation for measuring current and resistance, as well as for continuity tests. The integrated flashlight enables dark spots to be illuminated and the measuring tips can be changed easily, saving costs in the event of damage.
The three models in the Testo 750 range are the first voltage testers with an all-round LED display, which can be seen from any position and guarantees an ideal voltage indication due to its unique fibre optics. They meet the latest standards including EN61243-3:2010 and CAT IV, as well as providing the most important functions for voltage testing, continuity testing and rotating magnetic field measurement.
Finally, the Testo 745 non-contact voltage tester comes with a voltage range of up to 1000V and is ideal for the fast initial checking of any suspected fault sources, and provides clear visual and acoustic signals when voltage is detected. The device also has a low-pass filter for high-frequency interference signals and also meets IP67.
About RS Components
RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping more than 44,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.
Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2016 had revenues of £1.29bn.
For more information, please visit the website at www.rs-online.com.
Further information is available via these links:
Twitter: @RSElectronics; @alliedelec; @designsparkRS
RS Components on Linkedin
http://www.linkedin.com/company/rs-components
RS WeChat ID: RS_Components_CN
Relevant Links:
Electrocomponents plc
www.electrocomponents.com
RS Components
www.rs-online.com
DesignSpark
http://www.designspark.com