- Published 15 Mar 2024
- Last Modified 15 Mar 2024
- 5 min
Improving Electrical Safety in Commercial Properties with RCD Plugs and Sockets
Ensuring electrical safety in the workplace is crucial to protecting employees, customers, and equipment. Find out how RCD plugs enhance electrical safety.

The adoption of Residual Current Device (RCD) plugs and sockets plays a crucial role in ensuring electrical safety in commercial properties. Commercial sockets in Singapore intended for general use and/or by ordinary persons are required to have RCD protection, which protects the socket user in case of background leakage and fault.
These devices are not just supplementary equipment but essential tools that significantly enhance safety and protect against the dangers of electric shock.

Understanding RCD Technology
RCDs, such as Residual Current Circuit Breakers (RCCB), are designed to prevent fatal electric shocks by instantly detecting and responding to fault currents, which are electrical flows that deviate from their intended path.
When a discrepancy in the current flow is detected, indicating a potential electric shock risk, the RCD swiftly interrupts the power supply, thereby mitigating the hazard.
This rapid response is critical in commercial settings, where the risk of electrical accidents can be higher due to the complex wiring systems and the extensive heavy use of electrical equipment.
The Importance of RCDs in Commercial Settings
In the context of Singapore’s commercial sectors, the electrical safety challenges are manifold. The dense layout of commercial properties, combined with the tropical climate, increases the risk of electrical faults that can damage equipment, interrupt or cause power shortages, and even damage or cause death to users.
RCD plugs offer a layer of protection that goes beyond what traditional fuses and circuit breakers can provide, making them an indispensable component of any commercial property’s electrical safety protocol.
Furthermore, RCDs are in compliance with Singaporean electrical regulations, ensuring that commercial properties meet the necessary safety standards. For instance, the Consumer Product Safety Office’s (CPSO) Consumer Protection (Safety Requirements) Regulations specify several specific requirements related to socket outlets with RCD.
Types of RCDs
When outfitting your commercial space with RCD plugs, it’s imperative you choose the type that best suits your electrical needs. Common RCD types include:
- Socket Outlet RCDs: These are integrated directly into socket outlets, offering protection to any device plugged into them. This type is particularly beneficial for appliances that are more susceptible to electrical faults.
- Portable RCDs: Known for their flexibility, portable RCDs can be moved and used across different locations within a commercial space, providing targeted protection where it’s needed most.
- Inline RCDs: Ideal for use with extension cables or in areas exposed to moisture, inline RCDs safeguard against electrical faults in specific, potentially high-risk scenarios.
Benefits of Using RCD Plugs and Sockets in Commercial Properties
Implementing RCD plugs and sockets within commercial properties in Singapore brings a multitude of benefits.
Notably, they significantly reduce the risk of electric shock, enhancing the safety of both employees and customers.
Additionally, they protect valuable electrical appliances and infrastructure from potential damage caused by electrical faults, contributing to the longevity of these assets and reducing maintenance costs.
Implementing RCDs: Best Practices
Selecting the right RCD
- Assess the environment: Consider the specific characteristics of each area within the commercial property when choosing mains plugs and RCDs. Look at factors such as moisture levels, the presence of sensitive electronic equipment, or areas where electrical equipment is frequently used or changed.
- Determine the sensitivity required: RCDs come in various sensitivity ratings (e.g., 30 mA, 100 mA). Lower sensitivity RCDs (30 mA) offer greater protection, making them suitable for most areas. Higher sensitivity ratings may be appropriate for environments with larger electrical loads or where only protection against fire is required.
- Understand the types of RCDs available: Select between Type AC, A, F, or B RCDs based on the type of equipment and the electrical loads in your commercial property. For instance, Type A RCDs are suitable for protecting equipment with electronic components that can generate pulsating direct currents.
Installing RCDs
- Follow manufacturer guidelines: Ensure that RCDs are installed according to the manufacturer's instructions and in compliance with Singapore's electrical installation standards.
- Use qualified electricians: Only qualified and experienced electricians should install RCDs to ensure that the installation meets legal and safety standards.
- Consider placement: Install RCDs in accessible locations for easy testing and resetting. In environments with a high risk of water exposure, ensure that RCDs are placed in waterproof enclosures.
Testing, maintenance, and compliance
- Test regularly: Conduct regular electrical testing with multimeters to ensure RCDs are functioning correctly. The testing frequency can depend on the manufacturer's recommendation and the environment in which the RCD is used. A general guideline is to test them every three to six months.
- Use test buttons: Most RCDs come with a test button that simulates a fault to check if the RCD turns off the power as it should. This test should be performed at the intervals recommended by the manufacturer.
- Conduct professional inspections: In addition to routine testing, have RCDs inspected and tested by a qualified electrician at least once every two years to assess their condition and functionality.
- Keep records: Maintain a log of all testing and maintenance activities, including dates, findings, and any corrective actions taken. This record can be crucial for compliance purposes and in identifying patterns that may suggest the need for replacement or additional protective measures.
- Educate staff: Train staff on the importance of RCDs, how they work, and what to do in case an RCD trips. Awareness can significantly enhance the safety benefits of RCDs.
- Review and update: Regularly review the effectiveness of RCD protection in your commercial property. As new equipment is added or layouts change, reassess the need for additional RCDs or changes to existing installations.
Get the Electrical Protection You Need at RS Singapore

The role of RCD plugs and sockets in improving electrical safety in commercial settings cannot be overstated.
By integrating these devices into their electrical safety measures, property owners and managers in Singapore can significantly mitigate the risk of electric shock and electrical faults and ensure a safer working environment for everyone.
RS Singapore offers a wide range of RCD plugs and other electrical products, such as DC jacks and wall sockets, making it easier for commercial properties to find the right solutions for their safety needs. Browse selected brands below, or get in touch with us for more information on our products and services.
Popular RCD Plug Brands
Masterplug
Masterplug stands out with its circuit breaker plugs, offering robust protection against electrical faults. Their products are characterised by ease of use and durability, making them a preferred choice for enhancing electrical safety in diverse settings.
Powerbreaker
Powerbreaker’s RCD plugs are synonymous with quality and dependability. Specialising in residual current devices, they provide effective safeguards against electrical hazards, ensuring a safer environment in commercial properties.