Spirit Levels & Inclinometers
Spirit levels, also known as bubble levels or simply levels, are invaluable hand tools used to determine if a surface is perfectly horizontal (level) or vertical (plumb). From simple tasks like installing shelves to more complex projects like ensuring the accuracy of brickwork, spirit levels provide a quick and reliable way to achieve precise levelling.
Spirit levels operate using a liquid-filled vial, typically containing alcohol or mineral spirits, with an air bubble inside. Graduations or markings on the vial indicate when the bubble is centred, showing the user that it is level or plumb. Digital spirit levels offer the added convenience of a digital readout, providing even greater accuracy and eliminating guesswork. For best results, try to use the longest level that fits on either the horizontal or vertical (plumb) planes of the surface that is being checked.
An inclinometer, also known as a clinometer or slope meter, is a tool used for measuring angles of slope, tilt, or elevation relative to gravity. Unlike spirit levels, which primarily indicate levelness, inclinometers quantify the degree of inclination. Inclinometers utilise various measurement methods and can provide analogue or digital readouts. Traditional inclinometers often feature a gravity-based pendulum or a spirit vial, while modern electronic inclinometers employ sophisticated gyroscopes or accelerometers for enhanced precision.
Due to their higher accuracy, resolution, reliability, data storage capabilities, and ability to document measurements, electronic inclinometers are increasingly favoured over traditional spirit levels, particularly in applications demanding precise angle measurements and detailed record-keeping.
Difference Between Spirit Level and Inclinometer
While both spirit levels and inclinometers are used for measuring angles, they serve distinct purposes and operate on different principles:
A spirit level tool, also known as a bubble level gauge, primarily indicates whether a surface is perfectly horizontal (level) or vertical (plumb). It relies on a liquid-filled vial with an air bubble to show levelness.
In contrast, inclinometers measure the angle of a slope, tilt, or elevation relative to gravity, providing precise angle readings in degrees or percentages. While some bubble inclinometer models use liquid vials, electronic versions employ gyroscopes for enhanced accuracy.
Therefore, spirit level bubbles indicate level, while inclinometers quantify the degree of inclination, making them suitable for different types of measurement tasks.
Who Uses Spirit Levels and Inclinometers?
Spirit level tools and inclinometers are essential tools for professionals and DIYers across a wide range of industries and applications requiring precise angle measurements and levelling. Here are some key uses:
- Carpenters: Use spirit level rulers for ensuring level installations of framing, cabinetry, flooring, and other woodwork.
- Stonemasons: Rely on precision level gauges to maintain accurate alignment of stone during construction and masonry projects.
- Bricklayers: Employ spirit level indicators to ensure walls, foundations, and surfaces are perfectly level and plumb.
- Surveyors: Utilise inclinometers to measure slopes and angles for land surveying and construction planning.
Spirit Level Types
RS offers a diverse selection of spirit levels designed to meet the specific needs of various applications:
Straight Spirit Level
Designed for checking levelness over extended surfaces, straight spirit levels are long and flat. Their elongated design ensures accuracy over greater distances, making them ideal for tasks like installing long shelves, levelling floors, or aligning pipes.
Block Spirit Level
For general-purpose levelling tasks, block spirit levels are ideal. Their robust design and multiple vials allow for accurate horizontal and vertical measurements. The simplicity of block levels makes them a staple for DIY enthusiasts and professionals alike.
Box Section Spirit Level
Box section spirit levels offer enhanced rigidity, durability, and accuracy due to their reinforced box-shaped construction. The box-shaped profile prevents twisting and bending, maintaining accuracy even under stress and heavy use. This makes them ideal for construction sites and heavy-duty projects.
Torpedo Spirit Level
Torpedo spirit levels are compact, lightweight, and often magnetic, making them perfect for working in tight spaces or on metal surfaces. The tapered ends allow access to confined areas, and the magnetic strip ensures secure attachment to metal pipes or frames, freeing up hands for other tasks.
Bullseye Spirit Level
Also known as circular levels or surface levels, bullseye spirit levels are used for levelling surfaces in two dimensions simultaneously. Their circular vial allows for quick and easy levelling adjustments in any direction. They are particularly useful for levelling appliances or machinery on uneven surfaces, ensuring stability and proper operation.
Digital Spirit Level
With precise digital readouts, digital spirit levels eliminate guesswork and enhance accuracy. They are ideal for applications requiring high precision and detailed measurements. The digital display shows exact angle measurements, and some models include features like memory storage and audible alerts for specific angles.
Inclinometer Types
Manual Inclinometers
Manual inclinometers, also known as bubble inclinometers or analogue inclinometers, utilise a spirit level or pendulum to measure angles. They provide a straightforward and reliable method for basic slope determination without requiring a power source. These devices are user-friendly and ideal for field applications where simplicity and portability are key.
Digital Inclinometers
Equipped with electronic sensors (accelerometers or gyroscopes) and digital displays, digital inclinometers deliver highly accurate and easily readable angle measurements. The digital readout eliminates guesswork and enhances precision, making them suitable for applications demanding high accuracy and detailed readings. Many digital inclinometers also offer features like data logging, Bluetooth connectivity, and audible alerts.
MEMS Inclinometers
Micro-Electro-Mechanical Systems (MEMS) inclinometers employ microfabrication technology to create miniature sensors that measure tilt or inclination. Their miniature size, low power consumption, and high sensitivity make them ideal for precise angle detection in compact and demanding environments.
In-Place Inclinometers
Designed for permanent installation in boreholes or structures, in-place inclinometers continuously monitor movements in structures or soil. These devices provide long-term data on structural stability and ground movement, essential for monitoring critical infrastructure and geological formations.
In-Place Inclinometers with Settlement
These advanced in-place inclinometers measure both lateral movement and heave in boreholes or structures. Their data logging and real-time monitoring capabilities provide early warnings of potential failures, ensuring proactive maintenance and safety in critical applications.
Why Do Some Spirit Levels Have Two Bubbles?
A dual-vial system in spirit level tools indicates that the two vials function regardless of whether the level is placed on its top or bottom edge. This design enhances versatility, allowing for accurate readings in various orientations and confined spaces. Furthermore, it ensures consistent accuracy even if one surface of the level is slightly uneven.
Some spirit levels may also have a third vial set at a 45-degree angle for measuring diagonal slopes.
Considerations When Choosing Spirit Levels and Inclinometers
Accuracy
Assess accuracy by checking the tolerance, shown as a plus (+) or minus (-) value. A lower tolerance indicates higher precision, crucial for critical applications.
Resolution
Resolution refers to the smallest increment that the instrument can display or measure. Higher resolution is desirable for applications requiring fine adjustments or detailed measurements.
Bubble Size and Visibility
Larger bubbles offer better visibility, ensuring the bubble is easily seen within the marked lines. Liquid type influences bubble size, which may vary with temperature.
Vial Sensitivity
Vial sensitivity refers to the degree of tilt required to move the bubble a certain distance. Higher sensitivity vials respond more quickly to small changes in angle.
Colour
The coloured liquid within a spirit level enhances the visibility of the air bubble, making it easier to read measurements accurately. However, as prolonged sun exposure can cause the colour to fade, the bubble could become less visible. In turn, this could diminish reading precision.
Reading Lines
Clear reading lines on the tube or vial are essential for accurate measurements, preventing misinterpretations and ensuring reliable readings.
Construction and Durability
Robust construction, ideally with rubber-protected ends and a sturdy frame like aluminium, safeguards the delicate vial, especially on building sites. Additionally, look out for hand holds that enhance usability.
Additional Useful Features
Consider features that enhance usability and adaptability. For instance, a V-groove along the level's edge allows it to sit securely on pipes, preventing slippage during measurement. Similarly, the magnetic base in magnetic spirit levels allows for hands-free operation on steel surfaces, which is particularly convenient when working on structural steel or other metal frameworks.
Industrial Applications of Spirit Levels and Inclinometers
Construction and Civil Engineering
In construction, spirit levels are essential for ensuring walls, floors, and foundations are perfectly level and plumb. For example, bricklayers use box section spirit levels to ensure each course of bricks is level, maintaining structural integrity.
Inclinometers are also crucial for measuring slope angles in road construction and earthworks, ensuring proper drainage and stability.
Manufacturing and Machinery Installation
Manufacturing plants rely on precision level gauges to align machinery and equipment, ensuring optimal performance and preventing premature wear. Digital spirit levels are favoured for their high accuracy and digital readouts.
Inclinometers are also used to measure the tilt of conveyor systems and other moving parts, ensuring smooth and efficient operation.
Aerospace and Aviation
The aerospace industry uses inclinometers to measure the angles of aircraft components during assembly and maintenance, ensuring aerodynamic efficiency and safety. MEMS inclinometers are often preferred for their compact size and high accuracy. For example, they are used to calibrate flight control surfaces.
Spirit level indicators also come in useful for ensuring the levelness of aircraft floors and seating, providing passenger comfort and safety.
Telecommunications and Network Infrastructure
Telecommunication engineers use spirit level tools to ensure the vertical alignment of antenna masts and towers, optimising signal transmission and reception. For instance, torpedo spirit levels are often used to align satellite dishes and communication towers due to their compact size and magnetic base.
Meanwhile, inclinometers help to measure the tilt of utility poles and transmission lines, ensuring stability and preventing failures.
Rail and Transportation Infrastructure
Railroad maintenance crews rely on spirit levels to ensure the levelness of tracks and platforms, preventing derailments and ensuring passenger safety. Straight spirit levels are often used for their length and accuracy over extended surfaces.
Furthermore, to ensure structural integrity and prevent landslides, inclinometers are vital for measuring the slope of railway embankments and bridges.
Renewable Energy Installation
During solar panel installation, professionals use digital spirit levels to ensure panels are perfectly aligned for maximum energy capture. Bubble inclinometers are also employed to measure the angle of the panels relative to the sun.
Similarly, wind turbine installation also uses inclinometers to determine proper angle of blades.
Spirit Level Tool & Inclinometer Manufacturer, Supplier & Distributor in Singapore
RS Singapore is a trusted and leading manufacturer, supplier, and distributor of mechanical tools and parts, including spirit levels and inclinometers. We source our products from reputable brands like Stanley, Bahco, and SAM, ensuring high-quality options for our customers.
Beyond spirit levels and inclinometers, RS Singapore also provides a wide range of measurement products, such as data loggers and wind speed sensors, at competitive prices, serving as a one-stop shop for all your project needs. Whether you require a digital spirit level or a precision level gauge, RS Singapore has you covered.
Buy Spirit Levels and Inclinometers Online from RS Singapore
Discover the ease of browsing our extensive online catalogue, where you can select the ideal tools to meet your project needs. Enjoy the convenience of having your chosen items delivered directly to your doorstep, at a time that suits you. For detailed information regarding delivery times and associated fees, please consult our dedicated delivery information page.