Press Releases


RS Components introduces new RS Pro range of affordable rework tools for electronics design and repair engineers

New RS Pro workbench equipment offers highly affordable solutions including fume extractor and soldering and rework stations

Singapore, 26 June 2017:

RS Components (RS), the trading brand of Electrocomponents plc (LSE:ECM), the global distributor for engineers, is extending its competitively priced high-quality RS Pro range with a series of new workbench equipment, including a soldering station, a pair of rework stations and a fume extractor. These devices target repair work in production facilities, as well as in service environments or for engineers and technicians working in laboratories.

The first of the new additions is a 60W LCD Smart Soldering Station, which is supplied with a high-end alumina ceramic heating element for fast heat recovery. The station has built-in data memory to store and recall three frequently used temperatures, in Celsius or Fahrenheit, as well as a temperature calibration function. It also features an easy-to-read large backlit LCD screen, which is brightness and contrast adjustable, along with auto-sleep and wake, and tip calibration functions.

The second device is the SMD Rework Station, which is a hot-air station that also includes an attached heat gun holder. The temperature is microprocessor controlled with a closed-circuit design that provides high power and quick warm-up times. Other features include an LED display, adjustable airflow and air volume, and a brushless motor design with a noise level of less than 45dB.

The third product in the range is the two-in-one SMD Hot-Air Rework Station, which includes both hot-air gun and soldering iron and stand. Featuring two LED displays showing the respective SMD rework and the soldering temperature, the soldering iron has an alumina ceramic heating element, and the Hot-Air Rework Station is very quiet with a noise level of only 45dB. Additional features include microprocessor controlled temperature and a calibration function. Temperature and airflow are also adjustable for easy surface-mount and through-hole component rework.

The final product is the Fume Extractor Smoke Absorber, which is a versatile, portable fume extractor that can be placed on a workbench or desktop. It is ESD safe and absorbs up to 80% of noxious fumes quickly and safely using activated carbon filters, which are supplied separately. The unit has a quiet (42–45dB) built-in high-performance fan, delivering a maximum capacity of 1m3 per minute. Replacement filters are also available in the RS Pro workbench range.

As with all RS Pro products, the range offers customers a combination of quality, performance and value. All products are backed by the RS Seal of Approval, representing leading industry standards for audit, inspection, test and certification.

These new soldering products strengthen the existing comprehensive range of electronic workbench products and solutions that RS stocks.

About RS Components

RS Components and Allied Electronics are the trading brands of Electrocomponents plc, the global distributor for engineers. With operations in 32 countries, we offer more than 500,000 products through the internet, catalogues and at trade counters to over one million customers, shipping around 50,000 parcels a day. Our products, sourced from 2,500 leading suppliers, include electronic components, electrical, automation and control, and test and measurement equipment, and engineering tools and consumables.

Electrocomponents is listed on the London Stock Exchange and in the last financial year ended 31 March 2017 had revenues of £1.51bn.

For more information, please visit the website at www.rs-online.com.

Further information is available via these links:

Twitter: @RSElectronics; @alliedelec; @designsparkRS

RS Components on Linkedin
http://www.linkedin.com/company/rs-components

RS WeChat ID: RS_Components_CN

Relevant Links:

Electrocomponents plc
www.electrocomponents.com

RS Components
www.rs-online.com

DesignSpark
http://www.designspark.com